Advanced Waveform Utility
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CFReduction[:STATe] ON|OFF|1|0 [:SOURce]:RADio:AWU:WAVeform:CFReduction[:STATe]? |
SCPI Example |
|
Preset |
OFF |
State Saved |
Yes |
Ranges |
ON | OFF |
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CFReduction:PAPR <real> [:SOURce]:RADio:AWU:WAVeform:CFReduction:PAPR? |
SCPI Example |
|
Couplings |
Visible when the CFR is enabled. |
Preset |
8 |
State Saved |
Yes |
Min |
3 |
Max |
100 |
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CFReduction:MITeration <integer> [:SOURce]:RADio:AWU:WAVeform:CFReduction:MITeration? |
SCPI Example |
|
Couplings |
Visible when the CFR is enabled. |
Preset |
10 |
State Saved |
Yes |
Min |
1 |
Max |
1000 |
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CFReduction:CPERcent <real> [:SOURce]:RADio:AWU:WAVeform:CFReduction:CPERcent? |
SCPI Example |
|
Couplings |
Visible when the CFR is enabled. |
Preset |
100 |
State Saved |
Yes |
Min |
0 |
Max |
100 |
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CFReduction:BSIZe <integer> [:SOURce]:RADio:AWU:WAVeform:CFReduction:BSIZe? |
SCPI Example |
|
Couplings |
Visible when the CFR is enabled. |
Preset |
1000 |
State Saved |
Yes |
Min |
0 |
Max |
|
SCPI Command |
[:SOURce]:RADio:AWU:WAVeform:CFReduction:FMASk [:SOURce]:RADio:AWU:WAVeform:CFReduction:FMASk? |
SCPI Example |
|
Couplings |
Visible when the CFR is enabled. |
Preset |
-25,-100;-25,0;25,0;25,-100 |
State Saved |
Yes |